cancel
Showing results for 
Search instead for 
Did you mean: 

P-Nucleo-IHM001

marco siqueira
Associate II
Posted on June 05, 2018 at 22:29

Hello!! I intend to buy the P-Nucleo-IHM001 development kit and I would like to know if there are any free software that I can use to generate the code instead to use IAR.

Does the IAR free license work with the kit ?

Regards,

Túlio

1 REPLY 1
bluenow1896
Associate III
Posted on June 10, 2018 at 04:39

I have

P-Nucleo-IHM002 i

n hand and tried to play with.

I tried to use IAR permanent free version (with code size limitation of 32K), it works fine to build the generated code/project.

  I use MC SDK 5.1.0 , with STM32Cube 4.25

-Andy