cancel
Showing results for 
Search instead for 
Did you mean: 

LV53L0X outside

Kristoffer Gull
Associate II
Posted on June 17, 2018 at 21:30

are there any settings or lenses for the LV53L0X to help it cope with high ambiant light?

#lv53l0x #outside
3 REPLIES 3
Andy Saul
Associate II
Posted on June 20, 2018 at 13:10

Hi Kristoffer,

I'm not aware of any settings, but there are plenty of lenses available which will exclude light in the normal spectrum and allow a passband of light that will include the 940nm wavelength required. Check '940nm ir bandpass filter' as a search on Alibaba. I have the problem now (using VL53L1X) of finding a supplier that will make a custom moulded version! If anyone reading this knows of a supplier? The company that manufactures the oval lens supplied with the VL53L1X Nucleo breakout board kit would be brilliant to talk to!

Posted on June 21, 2018 at 19:49

Thanks for the response i have orderet a VL53L1X Kit to see if i get more range from it. what kind of range do you get in high ambient light, outsite with the  L1X?

Posted on June 21, 2018 at 20:05

I was under the impression that the recever part of the L0X was fitted withe an IR filter?