cancel
Showing results for 
Search instead for 
Did you mean: 

Do X-CUBE-MCSDK will support AC induction motors?

Damien Ratazy
Associate III
Posted on June 17, 2018 at 12:25

Hello,

For the moment, X-CUBE-MCSDK only support PMSMs and BLDC motors.

However, AC inductions motors are not supported yet, that's a shame because this kind of motor is still very present in the majority of industrial applications.

Do support of these motors are planned in a next version of X-CUBE-MCSDK?

Best regards, Damien

#acim-pmsm-bldc-x-cube-mcsdk
1 ACCEPTED SOLUTION

Accepted Solutions
Laurent Ca...
Lead II

Dear @Damien Ratazy​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

View solution in original post

5 REPLIES 5
Damien Ratazy
Associate III

Nobody at ST can answer me?

Claire O.
ST Employee

Hello,

Adding AC induction motor is part of our roadmap, but will not be added at short term. The development team is now more focused on new MCU addition.

Thanks and best regards,

Claire.

Damien Ratazy
Associate III

Thank you

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Lead II

Dear @Damien Ratazy​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards