cancel
Showing results for 
Search instead for 
Did you mean: 

AN1447 SOFTWARE DRIVER FOR 4-MULTIPLEXED LCD WITH A STANDARD ST62

Robert Dunn
Associate
Posted on June 18, 2018 at 14:12

The ST62 is obsolete. Is there a direct hardware replacement processor that would work in this application? Would the supplied software program for the ST62 be compatible with the new processor?

Thanks

#multiplex-lcd
1 REPLY 1
Posted on June 18, 2018 at 15:01

Really not sure there is any support for these 20+ year old families.

You should probably find a local ST rep or FAE and work with them to redesign/migrate the current use case, and understand your options.

You would likely need to find the source for your existing program, and recreate with current tools. A lot of DOS stuff isn't going to work at all with 64-bit Windows platforms.

An STM8 or STM32 (20-pin Cortex-M0) device should be able to driver available 7-segment displays

http://www.st.com/content/ccc/resource/technical/document/application_note/28/3c/6b/8b/3c/b9/45/c0/CD00004279.pdf/files/CD00004279.pdf/jcr:content/translations/en.CD00004279.pdf

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..