cancel
Showing results for 
Search instead for 
Did you mean: 

HCD_HandleTypeDef has 15 channels

ANDRE THEVENIN
Associate II
Posted on June 28, 2018 at 19:09

On STM32F7, the HS interface has 16 host channels.

But in the HAL, the HCD_HCTypeDef structure has only 15 HCD_HCTypeDef items.

Is this normal ?

Is this a bug ?

Is there an hidden reason ?

(I have an application which can have the need on the 16 channels because several devices will be connected via a hub)

#hcd_handletypedef #hcd_hctypedef
1 REPLY 1
Khouloud GARSI
Lead II
Posted on July 05, 2018 at 15:23

Hi

ANDRE.THEVENIN

?,

The issue is confirmed. We will fix it and update the &39&39stm32f7xx_hal_hcd.h&39&39 ASAP.

Many thanks for bringing this point to our attention

I also advise you to refer to the application note

https://www.st.com/resource/en/datasheet/stm32f479ii.pdf

 which will help you to build your own USB application based on an STM32 MCU. If you have any feedback about the application note, please do not hesitate to share it here:

https://community.st.com/0D50X00009XkVtDSAV

On the FAQs section, the following question was answered:

0690X0000060LC6QAM.png

Khouloud.