cancel
Showing results for 
Search instead for 
Did you mean: 

Timer in STM32L071 works correctly in Debug mode but incorrectly in Run mode

Truong Giang
Associate
Posted on July 10, 2018 at 08:23

Hello,

I designed a board using STM32L071KZU6. I am using HAL_TIM_Base. The timer works correctly in Debug mode. But when I use run mode without debug, the timer takes longer. (I set 5s but it is 1-2 min). What problem with it? Please review attached file with my configuration timer and clock. 

Thanks,

#debug #stm32_timers
0 REPLIES 0