2018-07-14 08:31 PM
Hi?From the <PM0075 Programming manual> ? P15?Mass Erase as below code is successful ?Now?I want to Main Flash memory programming , but I don't how to do it . Anybody Know?.....
Thanks!
/******************************************************/
STM32_flashUnlock();
FLASH_Status flashEraseAllOptionBytes_STM32(void)
{ FLASH_Status status = FLASH_COMPLETE; uint32_t flash_CR,flash_SR; flash_CR = readMem((uint32_t)&(FLASH->CR)); flash_CR |= CR_MER_Set; writeMem((uint32_t)&(FLASH->CR), flash_CR);flash_CR |= CR_STRT_Set;
writeMem((uint32_t)&(FLASH->CR), flash_CR);status = FLASH_WaitForLastOperation(((uint32_t)0x000B0000));
return 0x09;
}**********************************************************************/
#flash?-memory-programm #swd2018-08-09 09:30 PM