AutoDevKit Ecosystem

Ask questions and find answers on the AutoDevKit solution. Discuss voltage configurations, motor control, and AutoDevKitStudio programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

spc582b, wkpu RAM retention

I am developing an spc582bxx microcontroller using AutoDevKit Studio.The device needs to wake up from sleep (standby 0) via wkpu, and RAM data must be preserved when not in por mode.Therefore, I set the MC_PCU.PCONF2.B.STBY0 register before entering ...

John_Lee by Associate
  • 231 Views
  • 2 replies
  • 0 kudos

Resolved! How can I connect Lauterbach debugger to AEK-COM-10BASET?

Hello support team, I just received a new AEK-COM-10BASET board and trying to connect Lauterbach debugger with License module for MPC55xx. Question : How can I connect to the board through Lauterbach debugger & SW? Currently the SW (TRACE32) shows er...

apap_2-1777512866787.png apap_3-1777512975847.png apap_4-1777513103738.png
apap by Associate II
  • 199 Views
  • 2 replies
  • 0 kudos

Resolved! Cannot start AEK-COM-10BASET project from AutoDevKit 2.7

Hello,   I installed AutoDevKit Studio today and trying to create the AEK-COM-10BASET project from it.   Basically there is no option to create / start the AEK-COM-10BASET from AutoDevKit.   Also I tried to run Help > Install New Software > Work with...

1.jpg 2.jpg 3.jpg
apap by Associate II
  • 281 Views
  • 1 replies
  • 0 kudos

printf() error in AUTODEVKITSTUDIO

Hello Max VIZZINI,i'm facing issue in printf() in AUTODEVKITSTUDIO. im using printf() in the code after compiling im getting this error c:/autodevkitstudio-2.7.0/eclipse/plugins/com.st.tools.spc5.tools.gnu.gcc.ppcvle.win32_4.9.4.202511271245/toolchai...

Pooja1 by Associate II
  • 262 Views
  • 1 replies
  • 0 kudos

Resolved! Which MCAN should i select for CAN7 sys1

i'm using SPC58EC80E5 in that pin number 28 TX and 29 RX , in low level drivers configuration i dont know which MCAN to be select please help me and also if i want to configure any other CAN ,which MCAN i should select. below is my configuration scre...

Pooja1 by Associate II
  • 352 Views
  • 1 replies
  • 0 kudos

Resolved! AEK_POW_BMSNOTX (L9963E) cell voltage measurement

Evaluating the L9963E BCC chip for a BMS design, using the AEK_POW_BMSNOTX eval board together with AEK-MCU-C4MLIT1 (spc58ec) running the example BMS application as reference but seeing some odd results in the cell voltage readings.All readings are a...