Skip to main content
pichet
Associate II
May 21, 2003
Question

ST7Lite

  • May 21, 2003
  • 3 replies
  • 925 views
Posted on May 21, 2003 at 06:49

ST7Lite

This topic has been closed for replies.

3 replies

pichet
pichetAuthor
Associate II
May 18, 2003
Posted on May 19, 2003 at 01:37

Hello Anyboby

ST7Lite2 Current

I'm using an ST7lite2 and I need to save as much current as possible without an increase to cost.

The LVD detection is taking 0.2mA - Is there a better solution?

or should I use a external regulator with low voltage detection (But this will add to the cost of the final production)

JOM

itsmejatinus
Associate III
May 19, 2003
Posted on May 19, 2003 at 12:00

hello,

You can reduce the power consumption by using different power saving modes e.g. halt etc. . Its usage depends up on your application means which peripheral/s you want to use and other configuarations.

[ This message was edited by: Ranjeet on 19-05-2003 15:30 ]
stephanie
Visitor II
May 21, 2003
Posted on May 21, 2003 at 06:49

Don't forget also to configure all the unused I/Os as output at 0, to switch off all the unused peripherals, to switch off the ADC between 2 conversions if you don't need continuous conversions,...