Skip to main content
brian4
Associate III
December 3, 2003
Question

ST72F324J6 PWM Output pin

  • December 3, 2003
  • 3 replies
  • 734 views
Posted on December 03, 2003 at 12:51

ST72F324J6 PWM Output pin

This topic has been closed for replies.

3 replies

brian4
brian4Author
Associate III
December 3, 2003
Posted on December 03, 2003 at 07:08

Is the PWM output (OCMP1A) on Port F bit 4 effected by the DDR & the OR or does the the PWM write to the Pin/Pad directly.

I want an open drain output from the PWM.

Is this achievable?

[ This message was edited by: BrianM on 03-12-2003 11:39 ]
jatin
Visitor II
December 3, 2003
Posted on December 03, 2003 at 12:26

When an alternate function is used , alternate function takes priority our standard I/O programming. When signal is coming from on-chip peripheral, that pin is automatically configured in O/P mode(push-pull or open-drain) depending up on the peripheral used. So, it is not possible to change this configuration.

brian4
brian4Author
Associate III
December 3, 2003
Posted on December 03, 2003 at 12:51

Many thanks