Skip to main content
el98650
Associate II
May 22, 2003
Question

ST10 connected to DUART

  • May 22, 2003
  • 2 replies
  • 840 views
Posted on May 22, 2003 at 13:12

ST10 connected to DUART

This topic has been closed for replies.

2 replies

el98650
el98650Author
Associate II
May 21, 2003
Posted on May 21, 2003 at 13:06

Hey there,

I am trying to connect the st10f269 to a DUART froom Philips. The Duart accepts 8 bits which will come from the 16-bit data bus of the st10. The question is which Bits should be connected to the DUART. There is the obvious Software Solution to shift all characters i write so that the data to transmit is in the lower 8 bits, but i was wondering if there is a better solution. Any Ideas or hints are very appreciated.

el98650
el98650Author
Associate II
May 22, 2003
Posted on May 22, 2003 at 13:12

Ok figured it out myself.. If someone is interested in the solution just mail me..