Skip to main content
cdvehicle
Associate III
October 22, 2003
Question

some question

  • October 22, 2003
  • 2 replies
  • 605 views
Posted on October 22, 2003 at 10:41

some question

This topic has been closed for replies.

2 replies

cdvehicle
cdvehicleAuthor
Associate III
October 20, 2003
Posted on October 20, 2003 at 05:48

I use eval. schecmatic for my application(PC104-ISA). But I disable PCI, CPLD,ATX power, etc. The super I/O is SMCS's super IO. my question is can I use the eval. BIOS for my application. I have no BIOS soure.

stephen239955_st
Associate II
October 22, 2003
Posted on October 22, 2003 at 10:41

I am not confident that the Eval BIOS will work on your system. On the other hand, there is a package called the STPCKit that is located on this site that contains function source code and boot code for the STPC. There are also boot loader examples for WinCE and Linux. I suggest that you look at this package.

It is located on

http://www.stmcu.com/familiesdocs-75.html#Software - Development Package

and select the ''STPC Software Development Kit v1.0''.