Skip to main content
cyberguigou1
Associate II
June 4, 2003
Question

Communication PC, connection between RS232 / I2C by ST72264.

  • June 4, 2003
  • 3 replies
  • 868 views
Posted on June 04, 2003 at 07:02

Communication PC, connection between RS232 / I2C by ST72264.

This topic has been closed for replies.

3 replies

cyberguigou1
Associate II
June 3, 2003
Posted on June 03, 2003 at 08:13

Hello!

There is a program in language C to create a communication between the PC and my microcontroleur

ST72264. I shall want to exemplify there because I have many of bugs.

I found one doc on this site (AN969) but there are no examples of applications.

I shall be grateful to you for it if you could help me. I have now create the electronique card, it does not stay in me more than has to bring in the code of the program.

I inform you of the evolution of my project.

PS: I use the language C and my oscillator is of 8Mhz.

Thank you in advance.

itsmejatinus
Associate III
June 4, 2003
Posted on June 04, 2003 at 02:54

There is source code file available with this application note i.e. AN9zip. I'm here attaching it.

[ This message was edited by: Ranjeet on 04-06-2003 06:35 ]

________________

Attachments :

an969.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Ef&d=%2Fa%2F0X0000000bWV%2FEG8Ch6mdf_53lcr2U_u2uEA0y6VhamZUZRRA.I14Xww&asPdf=false
shreya
Visitor II
June 4, 2003
Posted on June 04, 2003 at 07:02

Hello,

In case you are using STVD7 2.5.2 with the MDT10-EMU3 you need the following patch, available on the net : ''ST72264Gx I2C correction for ST7MDT10-EMU3''.