Skip to main content
PGagn.1
Visitor II
August 24, 2020
Question

I guys, I was looking at the VL53L1X to detec water level in a manhole but it says the field of view is 15°-27°. Being in a manhole, this is way to wide. Any suggestions?

  • August 24, 2020
  • 2 replies
  • 716 views

The device I am developping on is on top of the manhole at 3-4 meters high and I need a 2-5 mm precision or so. I look forward for an idea. Looking at basic laser meters to take measurements, they all are capable of doing what I am looking for, but can't find what technology/sensor they use to make it happen... Any insight would be appreciated.

Thanks!

    This topic has been closed for replies.

    2 replies

    KnarfB
    Super User
    August 24, 2020

    The sensor has 16x16 SPADs internally, see data sheet. Its possible to use parts of that downto 4x4. This will narrow the FoV.

    Eleon BORLINI
    ST Employee
    September 3, 2020

    Hi @PGagn.1​ , did you solved you issue?

    -Eleon