Skip to main content
Associate II
March 3, 2026
Solved

LIV4F less sensitivity compared to MAX-M10S?

  • March 3, 2026
  • 3 replies
  • 600 views

Hi all,

to evaluate LIV4F and MAX-M10S, I use Mikroe "GNSS 9" and "MAX" click boards with a passive antenna (Quectel YEGT001W1AM).

While the MAX click board with the MAX-M10S gets a fix in less than one minute, the MAX 9 board with the LIV4F doesn't get a fix. Even when starting with an active antenna to get a fix and then switching to the passive antenna, the LIV4F stops operating. Sporadically, the GSV sentence shows then one or two weak (~20) signals while the MAX-M10S has >10 satellites with signals in the range 20..44.

From my understanding of the data sheets, both the LIV4F and MAX-M10S should have similar performance without an external LNA, isn't it?

Is there any known issue with the Mikroe GNSS 9 click board?

Or a possible misconfiguration of the LIV4F I could fix?

 

Best answer by bofh

@GalaxyQuest wrote:

Also looking at Mikroe GNSS9 board the RF line is powered, therefore, can you please remove R3 - 10 ohm to isolate the DC offset on RF_IN line and retest with passive antenna


R3 likely doesn't harm as stated above, but if there is really the 56pF capacitor C8, this would dampen the signal quite much. I'll remove it and report back.

 

3 replies

Andrew Neil
Super User
March 3, 2026

@bofh wrote:

Is there any known issue with the Mikroe GNSS 9 click board?


You'd have to ask Mikroe about that: it's their board - nothing to do with ST!

https://www.mikroe.com/support 

 


@bofh wrote:

Or a possible misconfiguration of the LIV4F I could fix?


You'd need to show your code to know that.

How to write your question to maximize your chances to find a solution

How to insert source code

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
bofhAuthor
Associate II
March 3, 2026

@Andrew Neil wrote:

You'd have to ask Mikroe about that: it's their board - nothing to do with ST!

asking for known issues in the ST community doesn't require that the product has "something to do" with ST. But MikroElektronika is official partner https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/MikroElektronika.html

To me, the board looks unsuspicious - maybe the 6.8n series inductor isn't perfect... I could add 3.9pF to GND to match the network shown in the X-NUCLEO-GNSS1A1 docs. Or remove it at all.

 


@Andrew Neil wrote:

@bofh wrote:

Or a possible misconfiguration of the LIV4F I could fix?


You'd need to show your code to know that.

no code by me, I'm using the LIV4F with factory settings.

bofhAuthor
Associate II
March 4, 2026

@unknown wrote:

It sounds like the LIV4F is struggling with passive antennas, even when the environment and placement seem fine, while the MAX-M10S works reliably. This could be due to the LIV4F’s sensitivity or internal LNA limitations.

If you need pin-compatible alternatives, here are two options often suggested:


this wording smells very much like AI slop. Even if not, it is inappropriate IMNSHO.

GNSS-LeaT
ST Employee
March 3, 2026

We don't normally support the Mikroe boards. However, I took a quick look at them on their web site. The GNSS 9 has an antenna power supply connected to the AON pin. If a passive antenna is being used, power should not be supplied to that pin or it will reduce performance.

The Max 2 board looks like it does not have an antenna power supply, which, to me, means it is designed for a passive antenna.

I recommend contacting Mikroe and asking their recommendations for using the GNSS 9 board with a passive antenna.

Technical Moderator
March 3, 2026

For my passive antenna test, I am using the EVB-LIV4F which is an ST Eval board, schematics are found here EVB LIV4F Schematics 

Also looking at Mikroe GNSS9 board the RF line is powered, therefore, can you please remove R3 - 10 ohm to isolate the DC offset on RF_IN line and retest with passive antenna

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
bofhAuthorBest answer
Associate II
March 3, 2026

@GalaxyQuest wrote:

Also looking at Mikroe GNSS9 board the RF line is powered, therefore, can you please remove R3 - 10 ohm to isolate the DC offset on RF_IN line and retest with passive antenna


R3 likely doesn't harm as stated above, but if there is really the 56pF capacitor C8, this would dampen the signal quite much. I'll remove it and report back.

 

Technical Moderator
March 3, 2026

Glad you were able to resolve this.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.