FAQ on Teseo-LIV3F

Document created by Francesco Virlinzi Employee on May 24, 2018Last modified by Francesco Virlinzi Employee on Jun 13, 2018
Version 5Show Document
  • View in full screen mode

Q) Where can I find information on Teseo-LIV3F

A) All the information are available on-line @ st.com

 

Q) Which constellations are supported on Teseo-LIV3F?

A) Teseo-LIV3F supports GPS, Glonass, Galileo, BeiDou and QZSS constellations

 

Q) Does Teseo-LIV3F support Assisted GNSS?

A) Yes. It does. Teseo-LIV3F support three Assisted GNSS: ST-AGNSS (no internet connection needed), Predictive AGNSS (internet connection needed) and RealTime-AGNSS (internet connection needed)

 

Q) Does Teseo-LIV3F support Raw Measurement data?

A) No it doesn't

 

Q) Is there an evaluation board?

A) Yes. There is the Teseo-LIV3F evaluation board. Have a look @ EVB-LIV3F

 

Q) Is there a prototyping board?

A) Yes. There is the Teseo-LIV3F prototyping board. Have a look @ X-Nucleo-GNSS1A1

 

Q) Is there an evaluation software PC tool?

A) Yes. There is the Teseo-Suite PC tool. Have a look @ Teseo-Suite

 

Q) Is there minimal order quantity?

A) No there is no minimal order quantity.

 

Q) Can the Teseo-LIV3F be re-programmed?

A) Yes, it can. Teseo-LIV3F supports firmware update on the field.

 

Q) Can the Teseo-LIV3F host customer-application/code?

A) No it can not. There is no SDK available on Teseo-LIV3F. Teseo-LIV3F isn't an open platform. It can be reprogrammed only with GNSS binary provided by ST

 

Q) Should I write Teseo-LIV3F driver from scratch?

A) No you shouldn't. ST provides ready-to-be-used STM32 driver (as binary and C-Code). They are avaialble @ X-Cube-GNSS1

Attachments

    Outcomes