STM32Nucleo Power Shield & Cube Monitor

Document created by Erwan LE SAINT Employee on Oct 25, 2017
Version 1Show Document
  • View in full screen mode

The X-NUCLEO-LPM01A is a 1.8 V to 3.3 V programmable power supply source with advanced power consumption measurement capability.

It performs consumption averaging (static measurement up to 200 mA) as well as real-time analysis (dynamic measurement up to 50 mA with 100 kHz bandwidth).

The X-NUCLEO-LPM01A operates either in standalone mode (using its LCD, joystick and button to display static measurements), or in controlled mode connected to host PC via USB (using the STM32CubeMonitor-Power software tool with its comprehensive graphical user interface).

It can be used to supply and measure the consumption of STM32 Nucleo-32, Nucleo-64 or Nucleo-144 boards, using Arduino connectors. Alternatively, it allows to supply and measure the consumption of any target connected by wires via the basic connector.

 

To lean more please visit www.st.com

Attachments

    Outcomes