STM32Cube Low-Layer APIs now deployed across the whole STM32 family

Document created by Thomas Borowczak Employee on Jul 13, 2017Last modified by Thomas Borowczak Employee on Jul 13, 2017
Version 2Show Document
  • View in full screen mode

 

We are pleased to announce that the STM32Cube Low Layer (LL) APIs, a light-weight, optimized, expert oriented set of APIs designed for both performance and runtime efficiency, are now fully deployed across all existing STM32 series. The Low-layer APIs are usable in standalone or in parallel with STM32Cube HALs (with a few restrictions) and are part of the corresponding STM32Cube packages. They also offer an easy migration e are pleased to announce that the STM32Cube Low Layer (LL) APIs, a light-weight, optimized, expert oriented set of APIs designed for both performance and runtime efficiency, are now fully deployed across all existing STM32 families. The Low-layer APIs are usable in standalone or in parallel with STM32Cube HALs (with a few restrictions) and are part of the corresponding STM32Cube packages.

They also offer an easy migration path from the STM32 standard peripheral libraries, and it has never been easier to migrate old SPL projects into the Cube environment.

* Newsbite available here

* Download the STM32Cube Low Layer APIs here

* How to easily port Low-Layer examples VIDEO

5 people found this helpful

Attachments

    Outcomes