How to run&debug from RAM without flashing flash STM32F1 devices (Keil)

Document created by Bogdan Golab on Jun 18, 2017Last modified by William Chang on May 5, 2018
Version 4Show Document
  • View in full screen mode

If you would like to debug&run program without flashing the device you can follow this procedure:

In this solution, You don't need to Configure the boot pin. not matter what Boot1, Boot0 are, It just works

 

step 1. Project->Options for Target STM32...->Target

target set

ROM is from 0x2000 0000 - 0x2000 4000 (16KB)

IRAM is from 0x2000 4000 -0x2000 8000 (16KB)

The exact value of ROM and RAM depend on your application.

 

step 2. Project->Options for Target STM32...->C/C++

-add the VECT_TAB_SRAM to the define field

-optionally you can change the Optimization to O0 or O1 when you want to avoid optimization at O3 level (this helps debugging code)

 

step 3. Project->Options for Target STM32...->Linker

-make sure the Use Memory Layout from Target Dialog is checked.

 

step 4. Project->Options for Target STM32...->Debug

-Copy the boot_ram.ini file to the project folder (e.g. C:\Users\..\MDK-ARM)

-select the boot_ram.ini as initialization file

-go to settings

make sure the value high lighted in green is exactly same as step 2 we have made.

 

Up until now, you are done!

To test it work or not, build the project then press Ctrl + F5.

 

 

Here is the boot_ram.ini file.

add the code below and save as boot_ram.ini file.

/****************************************************************/

/*----------------------------------------------------------------------------
Setup() configure PC & SP for RAM Boot
*----------------------------------------------------------------------------*/
FUNC void Setup (void) {
SP = _RDWORD(0x20000000); // Setup Stack Pointer
PC = _RDWORD(0x20000004); // Setup Program Counter

_WDWORD(0xE000ED08, 0x20000000);   //  Setup Vector Table Offset Register Bit 29 to one indicate that Vector Table is in SRAM region

}

 

FUNC void OnResetExec (void) { // executes upon software RESET without re-enter the Debug mode
Setup(); // Setup for Running
}

 

Setup(); // Setup for Running

/**************************************************************/

7 people found this helpful

Attachments

    Outcomes