WAND - Wireless Auto Note Device

Document created by fxanhkhoa on Nov 30, 2016Last modified by Oliver Beirne on Dec 7, 2016
Version 11Show Document
  • View in full screen mode

About this project :

WAND stands for Wireless Auto Note Device. And first version of WAND is an invisible drum, with a stick you can play the sound of the real drum. And this is a small and convenient toy for everyone.

For the future works, WAND can be illustrated as a device that is used for education or presentation tool. With the form of a laser pointer, teachers or presenters can use it to introduce their slides and also note, highlight or draw directly on the presentation area. Basically, to do those things, beside the hardware, WAND need a computer software that run at the same time with slideshow software (powerpoint …). Any note that are created by WAND need to be display on top of screen and save on a clone file.

 

 

 

Project info

Type : WAND can be illustrated as a device that is used for education or presentation tool

Progress :  my project is completed for first version. I still have work to do

Difficulty : Easy

License : UIT license

Upgrade : reducing floating and drifting

 

The Team :

 

Bui Anh Khoa

Alogrithm & Final System connecting and processingEmail: fxanhkhoa@gmail.com

Nguyen Manh Thao

Bluetooth paring and data collecting for androidEmail: 14520853@gm.uit.edu.vn

Le Chau Ngan

Android app interface & data processing to soundsEmail: 14520574@gm.uit.edu.vn

Dao Thanh Hai

Bluetooth IDB05A1 board processingEmail: thanhhai.ittalk@gmail.com

Nguyen Hoai Phong

Stick desgin and set up hardware

Email: 14520670@gm.uit.edu.vn

Bui Huy Hung

MPU6050 & HMC5883L proccesing

Email: 14520331@gm.uit.edu.vn

Ho Mai Kim Chi

MPU6050 & HMC5883L proccesing

Email: chimaikim.5495@gmail.com

Nguyen Thanh Hien

Drum Sounds finding

Email: 14520271@gm.uit.edu.vn

Ta Thoai An

Drum Sounds finding

Email: 14520082@gm.uit.edu.vn

Trinh Le Huy

Team mentorEmail: huytl@uit.edu.vn

Phan Dinh Duy

Team mentorEmail: duypd@uit.edu.vn

 

 

Things used in this project

 

Hardware components :


ST Nucleo Board1
MPU60501
HMC5883L1
MPU9150 (other choice)1this MPU9150 works better with smaller drifting
(recommended)

Hand tools and fabrication machines :

- Small and long wire (the smaller, the better)
- 3d printer

Software Tools :

Mbed.org

St-link ultilities 

 

Story

One day, our team gather in a room for daily meeting, but it is pretty boring, so we come up with an idea. That is this drum with small space consuming.

Attachments

 

- Attached files : WAND project - Google Drive 

Code

 

Schematics and circuit diagrams

  • The connection board
  • Link existing repository 

    WAND project - Google Drive 

CAD - Enclosures and custom parts

 

  • Attach file: 3 file Front, Back, Middle stick
  • Link existing repository

 WAND project - Google Drive 

 

THANK YOU FOR READING
2 people found this helpful

Outcomes