Skip navigation
All Places > University Community

INP PHELMA - Grenoble

Log in to follow, share, and participate in this community.

Recent Activity

Erwan LE SAINT
Transfo, un festival collaboratif, signé French Tech in The Alps Transfo est entièrement conçu par l’écosystème numérique alpin. Imaginé par le collectif French Tech in the Alps (400 membres), Transfo est ouvert à l’ensemble des acteurs du numérique, et au-delà. Avec un degré d’implication totalement libre. Sa particularité ? Il rassemble des… (Show more)
Erwan LE SAINT
If you have been wondering how difficult it would be to move your application to 32 bits, this hands-on workshop is for you. The availability of price-competitive, feature-rich and 'easy' to program 32-bit microcontrollers are just a few of the reasons why you should make the transition to a 32-bit platform.   Who should attend this workshop?… (Show more)
jean-christophe Toussaint
Hello The I2C bus is a very popular bus used for communication between a master (or multiple masters) and a single or multiple slave devices. This presentation is aimed at helping users to realize such a communication between a discovery board STM32L053 and an I2C pressure-temperature sensor MPL3115A2. This example was developed using the Keil…
in INP PHELMA - Grenoble
jean-christophe Toussaint
Hello The Serial Peripheral Interface (SPI) is a specification of serial, synchronous and full duplex communication between a master (or multiple masters) and a single or multiple slave devices. This presentation is aimed at helping users to realize such a communication between a Nucleo-STM32L476RG board and a SPI pressure-temperature-humidity…
in INP PHELMA - Grenoble