Skip navigation
All Places >

Switches and Multiplexers

Log in to follow, share, and participate in this community.

Recent Activity

borovschii.serghei
Hi! In my project I use STHV748. Pulser works with cable (50 Ohm) >10m long. To protect IC outputs from overvoltage I use next schematic. It is right? Can you recomend another variant?
in Switches and Multiplexers
Oleksandr Yaremchuk
Hello Communnity I use the eval board STEVAL-IME013V1 Input frequency 40kHz Transmission of a sin 40kHz signal from XDCR8 to LVOUT8 1:1 When the piezoelectric element UTR-1440K is switched on to the XDCR8 connector, the level of the received signal ~ 5mV When the UTR-1440K piezoelectric element is switched off from the XDCR8 connector, the level… (Show more)
in Switches and Multiplexers
yuan.leonel
Hello Communnity, I would like to know what is the minimum pulse frequency for STHV800 chip? Can it operate with 40-100 KHz piezoelectric transducer? Thank you.
in Switches and Multiplexers