Skip navigation
All Places >

STM8 MCUs

Announcement 1 Community platform frozen for maintenance
Announcement:Community platform frozen for maintenance
Log in to follow, share, and participate in this community.

Recent Activity

Szymon Panecki
Dear STM8 Community,   This is a very exciting moment for all of us. STM8 MCUs family was extended with a new device, which is named STM8S001J3. This new family member reshapes STM8 portoflio and takes it to the new level by introducing new, tiny, small form factor package - SO8N.  STM8S001J3 belongs to STM8S Value Line series. All STM8S Value… (Show more)
in STM8 MCUs
Vyacheslav Azarov
Hello anyone,   When compiling a program including Standard Peripheral Library in the output *.elf file, all unused modules was included. Does is SDCC the dead code elimination optimization and how to activate it?   Thanks in advance.
in STM8 MCUs
Vyacheslav Azarov
Hello everyone, Is it possible to get the values of the offset of variables in a frame, for use it in inline assembler? Or does is exist any other way to function arguments passing? As is possible in GNU GCC or COSMIC and other compilers. Thanks in advance.
in STM8 MCUs
Szymon Panecki
Dear STM8 fans,   Let me inform you, that STMicroelectronics extended hardware tools ecosystem available for STM8 MCUs by introducing two STM8 Nucleo-64 kits: NUCLEO-8L152R8 and NUCLEO-8S208RB.    Each of these Nucleo kits contains STM8 device in LQFP64 package (either STM8L152R8T6 with 64kB Flash or STM8S208RBT6 with 128kB Flash). All MCU's… (Show more)
in STM8 MCUs
edmond yun
Hello,   I have a question as to whether stm8L051F3 can do/calculate the floating operation or not, please help to let me know it,   currently I can't check it with printf function, because if using the library with tool option,  I got the size over error,   example :   float devided_Voltage = 0; float high_Voltage = 0; devided_Voltage =… (Show more)
in STM8 MCUs
Philipp Krause
ST has recently introduced 8-pin STM8 devices, while previously the lowest pin count available was 20.   I would like to see more STM8 devices with relatively low pin count, e.g. 12 or 14 pins. Since I intend to replace an Elan Microelectronics EM78P153A µC by an STM8, a compatible pinout would be great, but any 12- or 14-pin device would be… (Show more)
in STM8 MCUs
Hiren M
Hi, I would like to develop and sell one of my product using STM8S IC with STSW-STM8069 library from STVD and STVP. is there any licence for that?  if yes ,what is process to get licence for one and how much i have to pay for   Thanks Hiren
in STM8 MCUs
Vyacheslav Azarov
Hello everyone, Why does the STM8CubeMX prohibit the clocking of the RTC with a frequency of less than 1 MHz, not allowing to use of an LSE? I want made a watch! Thanks in advance.
in STM8 MCUs
devar devge
Hi, Where can ı find the standart library for stm8l001j3. The system offers to use the STSW-STM8016 standard peripheral library but this library does not include the stm8l001j3. I need help for this stuation. What are your offers? 
in STM8 MCUs
58916
Hi, I'm trying to use the ST Visual Develop with the Cosmic st8 32k compiler.  I install everything and build the project.  That all works fine.  When I try to connect to the Discovery board with the debugger using Swim ST-link, I receive the following error: Starting debug session...  -> Emulator reset (usb://usb)...   ** Connection error… (Show more)
in STM8 MCUs
Load more items