Skip navigation
All Places >

STM8 MCUs

Log in to follow, share, and participate in this community.

Recent Activity

David  Beltran Lacasa
We are trying to migrate a .lib library which we use with STM32F1 microcontrollers to an STM8S microcontroller. We would like to use a similar toolchain for the STM8S:     ToolChain for the STM32F1: Eclipse base IDE + Keil to code, compile and link uVision to debug.   ToolChain for the STM32F1: Eclipse base IDE + Cosmic to code compile and… (Show more)
in STM8 MCUs
Bjoern Smith
Hi everyone I'm working on a product usung STM8L052C6, annually number produced are around 50000 units.. The customer wants (for obvious reasons)to be able to lock the memory, which was easy enough, writing to the ROP byte.. But they also want to be able to unlock the chip again, I know the syntax, write AA to ROP, read EOP, write AA, read… (Show more)
in STM8 MCUs
Siva Sankar Chandika
Hi,    We are using STM8AF6246 micro-controller for our requirements. We are using samples provided by ST, while testing we have following scenarios. Auto Wake Up unit is working individually fine. Flash program also working individually (we did settings change for Flash program in ST debugger) good. If we combine both programs AWU and FLASH,… (Show more)
in STM8 MCUs
Brian Kling
In this one-hour webinar you'll get an introduction to ST PowerStudio, our software application for one-click comprehensive power and thermal analysis, helping you avoid long, complex and expensive application testing. It provides a very accurate estimation of power loss, junction and case temperatures, explores non-testable parameters and helps… (Show more)
atom
Hi friends,   We are using STM8L(STM8L051F3) and STM8S (STM8S003F3) for a project. I has been designed, developed and deployed. It works as expected - STM8L as a transmitter, wakes up from stand-by mode, collect some data, transmits it and goes back to stand-by mode and STM8S as a receiver, receives it and represents it visually. This set up has… (Show more)
in STM8 MCUs
marton.miklos
Hello all,   I would like to run a script when building a project in STVD before the preprocessor (the script generates a header).   Is there any way of doing this?
in STM8 MCUs
Chris Reynard
Hello,   I am looking at using a STM8L152 MCU in a product that detects and measures a combustible gas.   There are standards that govern how these products must operate, one of which is EN 50271:2010.   STM8L152 has a built-in watchdog feature but for this to satisfy the 'monitoring equipment' requirements of the standard it must operate… (Show more)
in STM8 MCUs
R V
Hi, I am trying to implement timer based on interrupt in STM8S003F3 using STVD and COSMIC C Compiler free version. I tried following this tutorial available on web Starting STM8 Microcontrollers - Page 19 of 27 - Embedded Lab . However, while modifying the stm8_interrupt_vector.c file for adding my TIM2_IRQHandler in the interrupt vector struct… (Show more)
in STM8 MCUs
R V
Hi, I want to use stm8s003f3 in my project. I was under the impression just like stm32 the ide and tool chain might be easily available. However, the same was not the case. I installed STVD as my IDE and wanted standard peripheral library for programming in C. But I wanted a toolchain for which I chose Cosmic C compiler. The thing is free, but,… (Show more)
in STM8 MCUs
Shailesh Patil
STVD 4.3.11v showing connection error while debugging software for STM8AL discovery board. 
in STM8 MCUs
Load more items