Skip navigation
All Places >

STM8 MCUs Community

Log in to follow, share, and participate in this community.

Recent Activity

Davy Jones
We have project in which FreeRTOS code is generated using CubeMx.   I see syntax is little different from documentation on FreeRTOS site.    How can I terminate and restart a particular task?   Main objective is  Terminate and restart a task causing HardFault Restart a crashed task     Want to know how to restarting a task in FreeRTOS code… (Show more)
in STM8 MCUs Community
patil.kalpesh
hi  i am kalpesh  , i new in stm8 . I want to learn how to program in stm8. Please tell me which software should i use? please help me . i have Stm8s003f3 20pin IC .    i search @ internet i didn't  get ?  please help me?     sorry for poor english   thank you
in STM8 MCUs Community
Vyacheslav Azarov
Hello everyone, Looking at the documents on the chips, I did not find any significant differences. Tell me please how they differ, and which model is preferable 003 or 903? Thanks.
in STM8 MCUs Community
Siva Sankar Chandika
Hi,    We are using STM8AF6246 micro-controller for our requirements. We are using samples provided by ST, while testing we have following scenarios. Auto Wake Up unit is working individually fine. Flash program also working individually (we did settings change for Flash program in ST debugger) good. If we combine both programs AWU and FLASH,… (Show more)
in STM8 MCUs Community
RAGHURAM A
ST-LINK Programmer few times its working ,mostly its displaying error message Failed to set configuration with MCU name STM8AF5289: SWIM error [30006]: Comm init error: chip does not answer    connections every thing ok  device will work rarely ,
in STM8 MCUs Community
Thomas Borowczak
We are proud to announce that more than 1 million of our STM32 Nucleo and STM32 & STM8 discovery boards have been delivered. This affordable kits have eased the access for thousands of developers to our STM8 and STM32 ARM Cortex-M families of microcontrollers and helped them to quickly start functional projects. Are you a STM32 Nucleo or STM32… (Show more)
Thomas Borowczak
  About this project :  STM8S SPL modified to be usable with the SDCC compiler   Project infoType : ST Standard Peripheral Library, usable with the SDCC compiler  Progress : complete and usable, the original example makefile still have to be updated to follow the standard shown in the test/template projects Difficulty : Easy / Intermediate /… (Show more)
patil.kalpesh
Hi I am new in st8s  micro controller . I am using IAR software to program the chip. When i click on download error occurred "Failed to set configuration with MCU name STM8S003F3: SWIM error [30006]: Comm init error: chip does not answer " Connection of STlink/V2  to chip Stlink/ V2 ----> Chip(STM8S003f3) GND  ----> GND(Pin no.7)… (Show more)
in STM8 MCUs Community
Philipp Krause
About two years ago, I did a comparison of C compilers for the STM8. It can now be found at http://www.colecovision.eu/stm8/compilers-2016.shtml.   I also redid the comparison and placed it at http://www.colecovision.eu/stm8/compilers.shtml.   For Cosmic, SDCC, IAR the current versions of the compilers were used. Due to difficulties with… (Show more)
in STM8 MCUs Community
jean-christophe Toussaint
Hello The Serial Peripheral Interface (SPI) is a specification of serial, synchronous and full duplex communication between a master (or multiple masters) and a single or multiple slave devices. This presentation is aimed at helping users to realize such a communication between a Nucleo-STM32L476RG board and a SPI pressure-temperature-humidity… (Show more)
Load more items