Skip navigation
All Places >

STM32 MCUs Community

Log in to follow, share, and participate in this community.

Recent Activity

jendoubi saif ddine
i have a html page that excute js functions so i add the needed file to fsdata.c but i can't manage to find the problem why it won't work  fs_open(&file, "/pie.html"); netconn_write(pAcceptedConnection, (const unsigned char*)(file.data), (size_t)file.len, NETCONN_NOCOPY); FsData.C #include "lwip/apps/fs.h" #include "lwip/def.h"   #define… (Show more)
in STM32 MCUs Community
Ronny Landsverk
I am generating stimuli for a CPLD circuit using my Discovery board - STM32F303VCT. I use CubeMX for peripheral/clock initialisation, and AC6 (Eclipse) for code. I am using TIM15 - PWM CH1/CH1N - One Pulse Mode - with RCR of some value, say N-1. The PWM signals are to run a half-bridge for an AC motor, and hence need to be complementary with a… (Show more)
in STM32 MCUs Community
Clive One
STM32L072 and LoRa Discovery Kit featuring Open LoRa module by Murata using STM32L072CZY6TR MCU   http://www.st.com/en/evaluation-tools/b-l072z-lrwan1.html    Features Ultra-low-power STM32L0 Series MCU, Cortex® -M0+ based with 192Kbytes of Flash memory, 20Kbytes of RAM, 6Kbytes of EEPROM, LCD, crystal-less USB, T-RNG, PCROP 157dB maximum link… (Show more)
in STM32 MCUs Community
jendoubi saif ddine
so this is my function that works fine when i add it to the script : send_text(pAcceptedConnection, " function drawChart() {var data = new google.visualization.DataTable();data.addColumn('string', 'Topping');data.addColumn('number', 'Slices');data.addRows([['Mushrooms', 3],['Onions', 2],['Olives', 1],['Zucchini', 4],['Pepperoni', 2]]);var options… (Show more)
in STM32 MCUs Community
S. Marsanne
P-L496G-CELL01 STM32L496 2G/3G Global Cellular to Cloud Discovery Pack Dedicated repository for related hints, tips, constructive questions and feedback.     STM32-C2C Global Turnkey solution: 1. 2G/3G Cellular modem with worldwide coverage from EMnify partner (MVNO) 2. Micro SIM socket and eSIM preprovisionned with Emnify complimentary… (Show more)
in STM32 MCUs Community
Radek R
Short example how to Configure CubeMX + SDIO + DMA +FatSF The example is applicable on devices with two DMA channels for SDIO (F2/F4/F7) 
in STM32 MCUs Community
Clive One
Got a red bar across the screen when I tried to submit this. Had answered one question and moved on to the next. Typing too fast...  
in STM32 MCUs Community
Thomas Borowczak
Thinking about going to 32 bit? The time is now! Join ST for a 1-hour webinar on how to move to 32-bitsFriday, April 20, 2018 from 11:00 to 12:00   Take advantage of the new advances that make it "easy" to program 32-bit microcontrollers, benefit from their cost-effectiveness and add new features to your application. This webinar will help…
in STM32 MCUs Community
Brian Kling
This community has been created for Drone application enthusiasts, developers, makers, universities, research institutes, engineers.   Everybody who is joining the community is encouraged to post their questions, and to share their experiences using photos, videos and any material regarding Drone applications based on ST devices or evaluation… (Show more)
Daniel Hassanian
If you have CubeMX v4.24 or above installed, you'll notice a new menu item named "select additional software components" under Projects menu. If you open it you'll see an empty window.   What is it you might ask? Well according to CubeMX user manual which is Here, in Section 5.10.1 you'll find that it's a new support for ARM Keil software packs.…
in STM32 MCUs Community
Load more items