Skip navigation
All Places >

MEMS and Sensors Forum

Log in to follow, share, and participate in this community.

Recent Activity

Roberto Preghenella
Dear all, I'm working on a LSM6DS3 chip. I have configured it to exploit the Activity/Inactivity recognition functionalities, and all is working. On the other hand, I'm not able to do the following and/or to find documentation references for that.   The chip recovers from the Inactivity state to the fully Active state if I shake it or tap it,… (Show more)
in MEMS and Sensors Forum
Ashish Pamula
Hi all, I'm working with the LIS3DSH accelerometer which is the accel2 click board on the raspberry pi. I was able to get the angles of x, y, and z-axis based on the binary reading and I was also able to determine the roll and pitch of the accelerometer based on the equation I found in the datasheet. The question I have is, how am I let it suppose… (Show more)
in MEMS and Sensors Forum
Gabriela Christy
How to calculate  Threshold value in "WAKE_UP_THS[5:0]" register in LSM6DS3 ? 
in MEMS and Sensors Forum
Riku Ueda
Hi, I'm in trouble about LSM330TR gyroscope power_down mode. I'm measuring the angular velocity every 100ms and when it isn't measuring, i'd like to implement power_down mode. I wrote such a program but the gyro data is just a random variant number.  When I use only normal mode, it works correctly. How long does it take to start up from… (Show more)
in MEMS and Sensors Forum
Rick Schue
I've been beating my head against the wall for the last couple of days trying to figure out why I cannot read registers at odd addresses through the LIS3DSH SPI interface with the nRF52832.  Byte accesses to even addresses work fine, but byte accesses to odd addresses always return the value of the register at the even address one location lower. … (Show more)
in MEMS and Sensors Forum
Edwin Hernandez
I need an outdoor window cover for the ToF VL53L1X. I’m planning to use it as a people detector sensor. I want to put it into an abs plastic case.   Here is the module that I obtain from Pololu Pololu - VL53L1X Time-of-Flight Distance Sensor Carrier with Voltage Regulator, 400cm Max 
in MEMS and Sensors Forum
Kristoffer Gull
are there any settings or lenses for the LV53L0X to help it cope with high ambiant light?
in MEMS and Sensors Forum
va vai
Hi, I am a novice trying to work on some sensors by connecting them to the STM32L476 nucleo 64 board. Currently I am trying to use the Time of flight sensor, VL53L0X breakout board, by connecting it at the I2C pins on the nucleo 64. Also, I am using system workbench to run the generated code. I am unable to understand as to how to include the… (Show more)
in MEMS and Sensors Forum
Subba Kodavalla
I am looking to use LIS2DE12 for my hobby project. Is there an application note on how to use LIS2DE12 to get speed? If so please share. 
in MEMS and Sensors Forum
vasilenko.sergey
Hello! I have looked at video about X-CUBE-MEMS1 ( Getting started with Unicleo-GUI for motion MEMS ... ). After that, I've installed Unicleo-GUI and in tab FW Managment I don't see any one  firmware for download on the board. In what correct folder, as it is said in the video, I need to unzip the packages en.x-cube-mems1.zip and… (Show more)
in MEMS and Sensors Forum
Load more items