All: I have been tinkering with the SensorTile to use as-is for some data logging applications. It wasn't my original intent, but it turned out to be so handy as-is I didn't see a need to make something ground-up for my very limited application. For this application the double-tap to start/stop didn't make sense, I wanted the device to…(Show moreShow less)
For those that migrated from the Rev 1.2.0 to 1.3.1 Sample code, there appears to be a significant change in how the drivers work that took me quite a while to isolate. Hoping you find this if you are doing some searching. There are two accelerometers on the SensorTile, one in the LSM6DS3 and one in the LSM303AGR. For the Rev 1.2.0 SensorTile…(Show moreShow less)
We use the HTS221 sensor to provide indoor temperature and humidity data in an IoT environmental monitor. In general it is easy to use. For power conservation we use the sensor in one-shot mode. We have found a scenario that will lock up the sensor's temperature and humidity measurements (sensor stops working). Scenario description: We tell…(Show moreShow less)