Skip navigation
All Places >

GNSS Positioning

Announcement 1 Community platform frozen for maintenance
Announcement:Community platform frozen for maintenance
Log in to follow, share, and participate in this community.

Recent Activity

Francesco Virlinzi
Q) Where can I find information on Teseo III solution? A) All the information are available on-line @ st.com   Q) Which constellations are supported on Teseo III? A) Teseo III supports GPS, Glonass, Galileo, BeiDou and QZSS   Q) Does Teseo III support Assisted GNSS? A) Yes. It does. Teseo III supports three Assisted GNSS: ST-AGNSS (no…
in GNSS Positioning
Francesco Virlinzi
Q) Where can I find information on Teseo-LIV3F A) All the information are available on-line @ st.com   Q) Which constellations are supported on Teseo-LIV3F? A) Teseo-LIV3F supports GPS, Glonass, Galileo, BeiDou and QZSS constellations   Q) Does Teseo-LIV3F support Assisted GNSS? A) Yes. It does. Teseo-LIV3F support three Assisted GNSS:…
in GNSS Positioning
Francesco Virlinzi
In the Teseo-LIV3F GNSS module the firmware configuration sits in the internal flash memory, in detail the configuration sits in a flash-section called NVM, which isn't overwritten during the firmware-update procedure.   It has been selected this design to guarantee a customer can raise a campaign of Teseo-LIV3F's update on the field with no care…
in GNSS Positioning
Francesco Virlinzi
Teseo-LIV3F supports two interfaces: UART and I2C and on both it provides the NMEA messages. In some applications, main-host could not care on NMEA stream at all and position awareness is required only when specific events happens. This is the so called I2C Positioning Sensor where Host reads the real-time position data, like any other sensor…
in GNSS Positioning
Francesco Virlinzi
X-NUCLEO-GNSS1A1 is the official prototyping platform of ST GNSS module Teseo-LIV3F.   It's the right tool to begin prototyping with Teseo-LIV3F because it provides access to all the I/O ports and signal the Teseo-LIV3F has, and it can be plugged on a STM32 Nucleo boards.       X-Nucleo-GNSS1A1 is member of STM32-ODE program which guarantees…
in GNSS Positioning
Francesco Virlinzi
The GNSS Positioning community has been created for GNSS/Positioning application enthusiasts, developers, makers, universities, research institutes, engineers.   STMicroelectronics is involved in Positioning applications since 1993     The first multi-constellation receivers in the world was  introduced in the market by STMicroelectronics with… (Show more)
in GNSS Positioning
Francesco Virlinzi
Question Trouble shooting Solution Connection My board is not detected by Teseo-Suite Verify the USB driver is correctly installed Verify the correct baud rate is configured in the Preference Menu Verify NMEA protocol is selected See topic on USB driver in Windows 10 X-Nucleo-GNSS1A1 Which binary use for my STM32 Nucleo board Launch Menu…
in GNSS Positioning
Francesco Virlinzi
ST GNSS receivers Teseo III and Teseo-LIV3F support GPS, Glonass, Galileo, BeiDou and QZSS constellation. In the ST standard configuration only GPS and Glonass are enabled. Final customers can configure the constellation they want based on their needed using the following commands   Configuration ST proprietary NMEA command GPS…
in GNSS Positioning