Skip navigation
All Places >

eDesignSuite

Announcement 1 Community platform frozen for maintenance
Announcement:Community platform frozen for maintenance
Log in to follow, share, and participate in this community.

Recent Activity

31253
Dear friends,                       I am in need of Pspice model for power factor controller L6563. please post ur suggestion for getting the same or is any other way to simulate the power factor correction?
in eDesignSuite
PINI BITON
Hi i working on the new project with viper06HS (115khz) -primary regulation . i have a problem , output voltage 12 v on the second winding drop with increase current(connecting load) when i used Light load the output is 12 (3mA) and when i start to increes the current (heavy load about 100mA) the output voltage is drop to 8.5v   the feedback… (Show more)
in eDesignSuite
Andrew Baker
I've just used EDesignSuite to design a Flyback PSU based around a L6566B As part of this, it has designed me a transformer, in around half a page of small, poorly formatted, dense, closely type text. How do I export this text so as to send it off to be made? It does not seem to be possible to get it out in any useful form? (Printed page is NOT… (Show more)
in eDesignSuite
Andrew Baker
Does ST have clear plans of what they are going to use to replace the Flash Configuration Application for the STNRGPF01 when Flash is finally killed off completely in 2020? 
in eDesignSuite
Andrew Baker
I am designing in a STNRGPF01? into a high-end consumer product. The product will also include an STM32 Arm processor. Is the information available to make it possible to have the Arm Processor upload the file into the STRNGPF01 from the ARM processor? This would allow a useful reduction in volume production costs, as well as allowing for easy… (Show more)
in eDesignSuite
Riccardo Villa
I'm logged in my.st.com  In my.st.com/analogsimulator/ I chose: Negative Buck-Boost and I click "Create" Button. I set correctly the input voltage, output voltage and output current. I chose the desired IC. I click on Start Design button, a new blank page opens. Initializing bar appears but the page closes after a while.   The browser… (Show more)
in eDesignSuite
elena brambilla
I want to design Qi wireless receiver with 7.5W output capacity. I will use device STWLC03JR.Can anyone suggest me compact designing criteria or specification for Induction coil.I have seen they are readily available from mouser and Digikey. I want to select as per 7.5W capacity.Share me link for such compact induction coil.
heaton.john
I am using the simulator for converting solar cells into 5V output to a USB plug. The simulator calculates a 648uH inductor which is VERY large, expensive and hard to find. How can I use a more standard inductor, like the 10uH stated in the datasheet for this design?
in eDesignSuite
Giovanni Bassi
Yesterday I started to work with the EVAL-IPFC01V1. Can I program the STNRGPF01 with the ST-LINK/V2 through the SWIM connector J2? Or I must use the UART J3 with the adapter in the box? In this case what is the correct FTDI cable model?   Best regards
in eDesignSuite
Load more items