fillon.nicolas

How to enable Read-out protection in your firmware using Cube library functions

Blog Post created by fillon.nicolas Employee on Feb 22, 2017

Hi,

 

Recently I had to write a sample code for a customer in order to turn on the read out protection of the flash to a level 1.

 

I did it for a STM32L15x Nucleo or Discovery board but it can be easily ported to another family of STM32.

 

The code is simple: if the level of readout protection is not set to 1, it will set it to level 1.

 

If the STM32 RDP is already at level 1 it will do nothing.

 

I have attached my code zipped.

 

Unzip it at:

 

STM32Cube_FW_L1_V1.6.0\Projects\STM32L152RE-Nucleo\Examples\FLASH

 

Use the IDE of your choice to build and load the code : IAR, Keil or SW4STM32.

Then once code is built and loaded.

 

Reset the board so that code will execute.

 

Now try to use ST-LINK Utility to access the flash: the tool will tell you that the read operation cannot be made because the readout protection has been activated.

 

BR,

 

Nicolas.

 

 

Here is the important part of the code to execute:

 

  /* Unlock the Flash to enable the flash control register access *************/
  HAL_FLASH_Unlock();

  /* Unlock the Options Bytes *************************************************/
  HAL_FLASH_OB_Unlock();

  /* Get pages write protection status ****************************************/
  HAL_FLASHEx_OBGetConfig(&OptionsBytesStruct);


  /* Check if readoutprtection is enabled ***********************/
  if((OptionsBytesStruct.RDPLevel) == OB_RDP_LEVEL_0)
  {
   
    OptionsBytesStruct.OptionType= OPTIONBYTE_RDP;
    OptionsBytesStruct.RDPLevel   = OB_RDP_LEVEL_1;
    if(HAL_FLASHEx_OBProgram(&OptionsBytesStruct) != HAL_OK)
    {
      /* Error occurred while options bytes programming. **********************/
      while (1)
      {

      }
    }

    /* Generate System Reset to load the new option byte values ***************/
    HAL_FLASH_OB_Launch();
  }

  /* Lock the Options Bytes *************************************************/
  HAL_FLASH_OB_Lock();

Attachments

Outcomes