• SPC5Studio 5.7.2 is available

    Dear All ,   SPC5Studio 5.7.2 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.7.2   For Mass Market: =========== - K2 ethernet support - Sphaero FlexPWM,SARADC,SPI - Dua...
    Erwan Y
    created by Erwan Y
  • SPC5Studio 5.5.0 is available

    Dear All ,   SPC5Studio 5.5.0 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.5.0     For Mass Market: =========== -Sphaero (SPC574S) starter kit Platform com...
    Erwan Y
    last modified by Erwan Y
  • SPC5Studio 5.7.1 is available

    Dear All ,   SPC5Studio 5.7.1 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.7.1   For Selected Customers: ================ - Network bugs fixing     Use ...
    Erwan Y
    last modified by Erwan Y
  • engineer needed asap

    I have a new project, targeting the SPC56, SPC5Studio.  I am exploring using this processor for DO-178 level B product.  I am looking for someone to get on retainer asap, to help me get my software tools set...
    Matthew Richardson
    last modified by Matthew Richardson
  • using FREERTOS,Prone to abnormal phenomenonI(IVOR1)

    Fast switch  machine (power on ---->power off ---->power on ---> power off-->.........) It is prone to the following problems (BootLoader +APP)  offset size is 0x40000 the PC 's value is 0x400...
    guo qiang
    last modified by guo qiang
  • SPC5Studio 5.6.0 is available

    Dear All ,   SPC5Studio 5.6.0 is available   *** Highlights ***   Here are the changes coming with SPC5Studio v5.6 For Mass Market: =========== -Integrated development Environment C/C++ Development T...
    Erwan Y
    last modified by Erwan Y
  • SPC5Studio 5.7.0 is available

    Dear All ,   SPC5Studio 5.7.0 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.7   For Mass Market:   =========== - Windriver support (see application leve...
    Erwan Y
    created by Erwan Y
  • RTC Standby Wakeup

    Hello Team. It's Shreedhar from Robert Bosch. I'm using SPC58EC80 microcontroller ,i want to program RTC module in standby mode such that it will wake after 5 hours . i'm facing problem to loading  RTCVAL in RT...
    Shreedhar Kandimath
    last modified by Shreedhar Kandimath
  • Secured update site DOWN for SPC5Studio : SOLVED

    Dear all ,   Update 09/11/2017 (11:36) : Server is UP.   For your information , our following update site server EEID0001 , selectedCustomers are currently DOWN. and SPC5Studio Marketplace is DOWN. we a...
    Erwan Y
    last modified by Erwan Y
  • SPC5Studio 5.4.0 is available

    Dear All ,   SPC5Studio 5.4.0 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.4.0  - Presets management fixes  - Add one shot preset for package component ...
    Erwan Y
    last modified by Erwan Y
  • SPC5Studio 5.3.0 is available

    Dear All ,   SPC5Studio 5.3.0 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.3.0 - Added FreeRTOS support for Bolero, K2, Velvety - New platform for SPC5BxL3-ADIS board ...
    Erwan Y
    last modified by Erwan Y
  • Linked *.с files in project workspace.

    Hi all. I use SPC5Studio 5.0.0 and have a problem with linking some C modules into project. I create link to files via menu Import->File System->From Directory and set checker "Create link in workspace". And the...
    Yuri Nagornii
    last modified by Yuri Nagornii
  • SPC570S50E1 problem with SWT.

    Hi all. I have a problem with SPC570S50E1.   SWT has been gonfigure with:   void swt_init(bool status) { INTC_PSR (SPC5_SWT_NUMBER) = INTC_PSR_ENABLE(INTC_PSR_CORE0, SPC5_SWT_PRIORITY); SWT_2.TO.R = 0x01...
    Yuri Nagornii
    last modified by Yuri Nagornii
  • SPC5Studio 5.3.2 is available

    Dear All ,   SPC5Studio 5.3.2 is available   *** Highlights *** Here are the changes coming with SPC5Studio v5.3.2 - Serial Read not fully working in Linflex_v1 driver   Here are the changes coming...
    Erwan Y
    created by Erwan Y
  • How i can add pin wizard to SPC570S-DISP project

    Hello! I wan add pinmap wizard to SPC570S-DISP project. Is this is possible?
    Vladimir Romanov
    last modified by Vladimir Romanov
  • SPC5Studio 5.2.3 is available

    Dear All ,   SPC5Studio 5.2.3 is available   *** Highlights *** - RLA SPC570Sxx clocktree update - RLA SPC570Sxx flexcan driver integration   - Several bugs and improvements, please refer to&#...
    Erwan Y
    last modified by Erwan Y
  • Write DataFlash

    Good day. I testing work SSD_C90FL driver. I d'not correct write data in to Data Flash. The recorded data are missing. How to fix it ? Best regards.
    Alexey Potyomkin
    last modified by Alexey Potyomkin